ECAT.RXIRQTIME

Description

This parameter allows viewing and recording of the Distributed Clock (DC) time when the drive received the output packet (RxPDO). This is the same time as the SM2 event.

Context

See EtherCAT Drive Synchronization.

Versions

Action Version Notes
Implemented 02-07-04-000  

General Information

Type

Read Only

Units

ns

Range

0 to 4,294,967,295 ns

Default Value

N/A

Data Type

Integer
See Also ECAT.RXDONETIME, ECAT.POSLOOPTIME, ECAT.TXDONETIME, ECAT.SYNC0TIME

Stored in Non-Volatile Memory

No

Variants Supported

EtherCAT variants: AKD2G-SPE